hi
I am studying the usage of the 2944.
In the manual of the 2944, I learned that the four UARTs have different roles, as shown in the figure.
Question 1: Are the four UARTs referring to MSS UART, DSS UART, BSS UART, and RS232UART?
Question 2: I compared the EVM schematic and the MSS UART connected to XDS110 should be responsible for debugging registers mentioned in the screenshot, am I correct?
Question 3: What functions do the other three UARTs serve? Why is the DSS UART in a disconnected state on the EVM?
Simon