Other Parts Discussed in Thread: AWR1243
Hello:
The material corresponding to T04756616 is MMWCAS-DSP-EVM. The customer encountered the following problems during the test, and he hopes TI can return and replace the goods. Please check the attachment.
Summary of the problems encountered in the cascade board
一、Problems encountered
According to the guidance of the official document, the downloaded mmwave_studio script is run: Cascade_Configuration_MIMO.lua and Cascade_Capture.lua, and the running results are shown in the figure:

图1 mmwave_studio运行结果
Using WinSCP to view SSD, only a new folder and no data under the folder, as shown in the figure:
Figure 2 There is no radar echo data under the folder in the SSD
The DSP board status is as shown below:

图3 DSP板运行状态图
二、Forum information
Check the related problems and solutions to the forum, mainly refer to the following two articles: AWR1243: Cascade EVM-No data files in SSD after successful running script Cascade_Capture.lua-Sensor Forum-Sensor-TI E2E Support Forum and MMWCAS-DSP-EVM: Cascade EVM-No data files in SSD after successful running script Cascade_Capture.lua-Sensor Forum-Sensor-TI E2E Support Forum:
For the first forum, mmwave_studio error is shown in the figure:

Figure 4, mmwave _ studio, reported an error