This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-DSP-EVM: 利用级联板采集数据的时候上位机报错提示无法收到“CAPTURE_RESPONSE_ACK”信号

Part Number: MMWCAS-DSP-EVM


您好,我们在使用MMWCAS-DSP-EVM以及MMWCAS-RF-EVM板的时候,用mmwavestudio上位机进行雷达数据的采集,利用了master、slave1和slave3这三个通道,使用官方提供的Cascade_Configuration_MIMO_Test.lua脚本进行配置,配置成功后利用Cascade_Capture.lua脚本进行雷达数据的采集,但是上位机在采集时出现了“TDA Stop Record ACK not received!”的报错。配置成功后利用Capture脚本进行数据采集时的具体打印信息如下:

[19:03:17]  Loops Remaining : 10
[19:03:17]  Starting TDA ARM...
[19:03:17]  [RadarAPI]: ar1.TDACaptureCard_StartRecord_mult(1, 0, 0, Cascade_Capture_22xx, 0)
[19:03:17]  Device 0 - Configuring TDA with Width : 2000 and Height : 1536
[19:03:17]  [RadarAPI]: Device 0 - setWidthAndHeight Status: Passed
[19:03:17]  [RadarAPI]: Device 1 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0 
[19:03:17]  Device 1 - Configuring TDA with Width : 0 and Height : 0
[19:03:17]  [RadarAPI]: Device 1 - setWidthAndHeight Status: Passed
[19:03:17]  Device 2 - Configuring TDA with Width : 0 and Height : 0
[19:03:17]  [RadarAPI]: Device 2 - setWidthAndHeight Status: Passed
[19:03:17]  Device 3 - Configuring TDA with Width : 2000 and Height : 1536
[19:03:17]  [RadarAPI]: Device 3 - setWidthAndHeight Status: Passed
[19:03:17]  [RadarAPI]: Device 8 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0 
[19:03:17]  Sending Frame Periodicity of 100 to TDA..
[19:03:17]  [RadarAPI]: Status: Passed. Frame Periodicity sent to TDA
[19:03:17]  [RadarAPI]: Device 32 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0 
[19:03:17]  Sending Capture Directory with name /mnt/ssd/Cascade_Capture_22xx to TDA..
[19:03:17]  [RadarAPI]: Status: Passed. Capture Directory sent to TDA
[19:03:17]  [RadarAPI]: Device 32 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0 
[19:03:17]  Sending File Allocation of 0 files to TDA..
[19:03:17]  [RadarAPI]: Status: Passed. File Allocation sent to TDA
[19:03:17]  [RadarAPI]: Device 32 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0 
[19:03:17]  Sending Enable Data Packaging (0 - 16-bit; 1 - 12-bit) with value of 0 to TDA..
[19:03:17]  [RadarAPI]: Status: Passed. Enable Data Packaging sent to TDA
[19:03:17]  [RadarAPI]: Device 32 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0 
[19:03:17]  Sending Number of frames to capture with value of 0 to TDA..
[19:03:17]  [RadarAPI]: Status: Passed. Number of frames to capture sent to TDA
[19:03:17]  [RadarAPI]: Device 32 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0 
[19:03:17]  [RadarAPI]: Status: Passed for notifying TDA about Creating Application
[19:03:17]  [RadarAPI]: Device 32 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0 
[19:03:17]  [RadarAPI]: Status: Passed for notifying TDA about Start Frame
[19:03:17]  [RadarAPI]: Device 32 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0 
[19:03:17]  TDA ARM Successful
[19:03:17]  Starting Frame Trigger sequence...
[19:03:17]  [RadarAPI]: ar1.StartFrame_mult(8)
[19:03:18]  [RadarAPI]: Status: Passed
[19:03:18]  Device 4 : Start Frame Successful
[19:03:18]  [RadarAPI]: ar1.StartFrame_mult(1)
[19:03:18]  [DeviceId-3] Frame start async event received!
[19:03:18]  [RadarAPI]: Status: Passed
[19:03:18]  Device 1 : Start Frame Successful
[19:03:18]  Capturing AWR device data to the TDA SSD...
[19:03:18]  [RadarAPI]: Frame Ended
[19:03:18]  [DeviceId-0] Frame start async event received!
[19:03:18]  [DeviceId-3] Frame End async event received!
[19:03:18]  [DeviceId-0] Frame End async event received!
[19:03:18]  Status: Passed for notifying TDA about Stop Frame
[19:03:20]  Capture sequence completed...
[19:03:22]  Loops Remaining : 9
[19:03:22]  Starting TDA ARM...
[19:03:22]  [RadarAPI]: ar1.TDACaptureCard_StartRecord_mult(1, 0, 0, Cascade_Capture_22xx, 0)
[19:03:22]  Device 0 - Configuring TDA with Width : 2000 and Height : 1536
[19:03:22]  [RadarAPI]: Device 0 - setWidthAndHeight Status: Passed
[19:03:22]  Device 1 - Configuring TDA with Width : 0 and Height : 0
[19:03:22]  [RadarAPI]: Device 1 - setWidthAndHeight Status: Passed
[19:03:22]  Device 2 - Configuring TDA with Width : 0 and Height : 0
[19:03:22]  [RadarAPI]: Device 2 - setWidthAndHeight Status: Passed
[19:03:22]  Device 3 - Configuring TDA with Width : 2000 and Height : 1536
[19:03:22]  [RadarAPI]: Device 3 - setWidthAndHeight Status: Passed
[19:03:22]  Sending Frame Periodicity of 100 to TDA..
[19:03:22]  [RadarAPI]: Status: Passed. Frame Periodicity sent to TDA
[19:03:25]  TDA Stop Record ACK not received!
[19:03:25]  Frame Periodicity Response from Capture Card timed out!!
[19:03:25]  TDA ARM Failed
[19:03:25]  
[19:03:25]  ***Script completed successfully.***

我们对板子的部分地区进行了重新焊接,想知道出现这种情况的原因是什么呢?具体是板子的哪一部分模块可能出了问题呢?