hi,
My hardware is AWRL1432BOOST. when I use SDK5.4\tools\visualizer to run the given demo(such as motion detection, presence detection, and tracking demo) is ok, but when I run the KTO demo and bike_radar demo goes wrong, I want to know that the SDK5.4\tools\visualizer can run this demo? Can this visualizer only run some demos? Not all demos can see point clouds in this visualizer.
Why don't I use the special visualizer in radar toolbox to see the effect, I want to see all kinds of information of point cloud under this demo, such as distance resolution and angle resolution.
The following are the problems encountered:

the KTO demo, flash is ok.
then I reset the radar, and Re-supply power. And I change the SOP to the function mode as the tips need.


best wishes,