This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWRL1432BOOST: SDK5.4\tools\visualizer, Run the KTO demo and bike_radar demo goes wrong. "error in halting device,please try again"

Part Number: AWRL1432BOOST


hi,

    My hardware is AWRL1432BOOST. when I use SDK5.4\tools\visualizer to run the given demo(such as motion detection, presence detection, and tracking demo) is ok, but when I run the KTO demo and bike_radar demo goes wrong, I want to know that the SDK5.4\tools\visualizer can run this demo? Can this visualizer only run some demos? Not all demos can see point clouds in this visualizer.

  Why don't I use the special visualizer in radar toolbox to see the effect, I want to see all kinds of information of point cloud under this demo, such as distance resolution and angle resolution.

  The following are the problems encountered:

  

the KTO demo, flash is ok.

then I reset the radar, and Re-supply power. And I change the SOP to the function mode as the tips need.

 

best wishes,