This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: 一些相关问题

Part Number: AWR2944


profile_advanced_chirp_advanced_frame_DDMA_awr2944_test.cfg

基础:
1.硬件为AWR2944 EVM;
2.官方固件:awr2944_mmw_demoDDM.appimage、sbl_qspi.release.tiimage;
3.基于参考配置profile_advanced_chirp_advanced_frame_DDMA_awr2944.cfg修改成profile_advanced_chirp_advanced_frame_DDMA_awr2944_test.cfg;

预期:
AWR2944 EVM的Tx3、Tx4发射,DDMA工作模式,1个空带.

问题:
目标的+速度正确,但是-速度出现在±20m/s左右。

请问profile_advanced_chirp_advanced_frame_DDMA_awr2944_test.cfg哪里有问题,谢谢!

问题2

make file 怎么用?