This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: 使用嵌入式设备连接雷达,并显示由雷达传回的数据

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: IWR1642

以IWR1642BOOST,使用毫米波雷达工具箱3.6.0版本中的driver Vital Signs示例。参考适用于TI mmWave sensor平台的配置随启动加载的方式 - 汽车 - 技术文章 - E2ETm 设计支持这篇,可以尝试将配置固化在板子上,无需使用嵌入式设备发送配置,然而对于嵌入式设备的USB设备虚拟成两个COM口来对接一个有用的数据传输口和一个无用(已固化)的COM口并不方便。请问如何直接屏蔽掉配置发送端口?我在使用STM32设备。

另外,我并没有在手册中发现USB传输数据的格式,我需要提取到来自IWR1642BOOST向上位机发送的phaseWfm(经过带通滤波器后可分离除心率波形和呼吸波形),BreathingRate以及heartRate,所以想知道IWR1642BOOST在driver Vital Signs示例下,USB发送数据的格式如何,并参考USB发送的格式,提取我所需要的数据并完成显示工作。

  • 你好,

    IWR1642BOOST上的 TM4C1294NCPDTT3(xds110功能)转换了两个uart口输出,如果你只要一个串口,建议不使用 TM4C1294NCPDTT3,断开uart和 TM4C1294NCPDTT3
    的连接,直接输出uart信号给STM32。

    Thanks,

    Chris

  • 你好,

    使用毫米波雷达工具箱3.6.0版本中的driver Vital Signs示例,固化到IWR1642上,是否有更相似的教程可以提供。

    查询原理图得知UART经过100K上拉电阻到3.3V是否可以直接接入到电源电压为3.3V的STM32设备上。

    感谢

  • 使用毫米波雷达工具箱3.6.0版本中的driver Vital Signs示例,固化到IWR1642上,是否有更相似的教程可以提供。

    其他固化配置的demo都是基于mmw demo的,radar_toolbox_2_10_00_04\source\ti\examples\Fundamentals\Hard_Coded_Config

    查询原理图得知UART经过100K上拉电阻到3.3V是否可以直接接入到电源电压为3.3V的STM32设备上。

    我不清楚STM32设备,需要你自己评估。

    Thanks,

    Chris

  • 您好,我将IWR1642BOOST评估板上的R166和R169使用0欧电阻短接,此时我仍然使用XDS110连接到PC上,在使用GUI配置雷达时,可以在RS232_TX和RX上读取到PC的配置信息和IWR1642回传的确认信息。但是当雷达配置完毕启动后,UART线路上就没有信息传输了。而GUI上仍然有正确的信息回传。那么您之前所说的UART是什么?我看原理图发现 TM4C1294NCPDTT3和IWR1642的连接基本只有这个UART和JTAG,那么雷达回传的数据应该在哪里可以接收到,即USB中的921600波特率的数据口

    感谢

  • 你好,

    mmw demo使用一个uart作为cli接口,另外一个uart的TX作为结果输出。请在M4C1294NCPDTT3的连接上再找一下。

    Thanks,

    Chris