Part Number: AWR2944EVM
Hi, TI`s engineers
I have met the below question when I go ahead with AWR2944EVM,
串口和SPI链接失败。具体的出现的现象如下图所示:
Best regards,
J.R.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AWR2944EVM
Hi, TI`s engineers
I have met the below question when I go ahead with AWR2944EVM,
串口和SPI链接失败。具体的出现的现象如下图所示:
Best regards,
J.R.
感谢您对TI产品的关注!
关于你的咨询,对于这个error。
1. 你是否按照评估板的user guide内的操作进行的。
2. 硬件连接是否有问题。
3. PC的防火墙和杀毒软件是否关闭
4. 你需要DAC1000和mmWave studio软件连接。
Root Cause
1.Incorrect physical connections
2.Another program may be accessing the "Application /UART" COM port
3.The SOP pins are not set correctly
Solution
Check all physical connections (USB cables, power cables)
Close any other programs that may be accessing the serial ports for the mmWave device
Ensure that both SOP0 and SOP1 are jumpered across or set to "ON" position
1588.DCA1000 Debugging Handbook.pdf
下面几个过去的案例与你的问题一致,你看下。
e2e.ti.com/.../iwr6843isk-connection-error-radarapi-error-connection-failed-calling_connecttarget-returned-3
e2e.ti.com/.../awr1642boost-radarapi-error-connection-failed-calling_connecttarget-returned-3