Part Number: IWR1843
硬件:Iwr1843(pcb是自己设计的),xds200
软件:CCS 12.6.0,使用的是官方的demo,Multi_Gesture_and_Motion_Detection_18xx

1843通过XDS200连接到PC,工程的编译已通过,生成multi_gesture_18xx_ods_mss.out文件(2.8M),test Connection已成功,进入debug模式时出现下面的错误代码:
Cortex_R4_0: Trouble Writing Memory Block at 0x0 on Page 0 of Length 0x3c: (Error -1065 @ 0x0) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 12.6.0.00029)
Cortex_R4_0: File Loader: Verification failed: Target failed to write 0x00000000
Cortex_R4_0: GEL: File: D:\HGesture\Gesture_recognition\multi_gesture_18xx_ods_mss\Debug\multi_gesture_18xx_ods_mss.out: Load failed.
怀疑可能是gel文件配置错误,检查了target Configuration,发现DAP的配置文件是xwr16xx,这个配置文件是否可能就是错误的主因?在gel文件夹下面并没有发现xwr18xx的gel配置文件。