Other Parts Discussed in Thread: UNIFLASH, AWR2243, DCA1000EVM
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
之前没连接上SPI报的下面这个错误,然后我尝试用uniflash擦除,发现又报了command format is not a valid command. internal error.的错误
你好,
使用uniflash尝试擦除flash的时候,SOP是否设置为101?
使用mmwave studio的时候,SOP是否设置为011?
Thanks,
Chris
使用uniflash前设置了SOP为101,然后按了那个NRST按键,如下图所示
还在?请问可以帮我一下吗,
我已经使用uniflash前设置了SOP为101,然后按了那个NRST按键,如下图所示,但是还是不行,还是报同样的错误
已解决擦除flash的问题,用更旧的版本进行擦除就可以了,但是擦除后重连发现还是会有 MSS Power Up async event was not received!的报错,请问是怎么回事呢?
你好,
这是一个新板子么?之前有正常使用过么?
Thanks,
Chris
对,这是一个新的板子,还有一个问题是我只给awr2243雷达模块供电,但是没有单独给DCA1000供电,它们之间用跳线连接,这样没有问题吧,更详细的情况和问题描述请看下面的ppt文件
你好,
你能否尝试给DCA1000EVM也单独供电,看问题是否有变化?
Thanks,
Chris
我正在从网上购买并且尝试,并且请问可以帮忙看一下发给您的PPT文件里面的问题和情况描述吗?帮忙看看有什么问题是遗漏的
我给DCA1000EVM也单独供电了,发现还是不行,不知道连No.of Devices Detected不管怎么刷新都显示为零,我是连接并且打开雷达后过一会儿后才打开mmwavestudio的
你好,
DCA1000EVM上usb是连载radar接口上的么?
Thanks,
Chris