This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843BOOST: 关于IWR1843配置BPM发射模式的疑问

Part Number: IWR1843BOOST
Other Parts Discussed in Thread: IWR1843

我现在需要实现IWR1843的BPM发射模式的配置。按照我的理解,以IWR1843 使能TX0和TX2为例,在相同的ADC数量、Chirp数量的情况下,设置为TDM发射模式得到的bin文件大小应该是设置为BPM发射模式得到的bin文件大小的2倍。

我设置的是ADC数量256,1帧的Chirp数量128,50帧。按照这个设置计算的话,TDM得到的文件大小应该为50*8*256*128*16*2/8/1024/1024=50MB。BPM得到的文件大小应该为50*4*256*128*16*2/8/1024/1024=25MB。但为什么BPM得到的是50MB,我不理解。

以下是我配置BPM的过程:

1. 使能移相器

2. 配置Chirp的chirp 0

3. 配置Chirp的chirp 1

4. 配置BPM的chirp 0

5. 配置BPM的chirp 1

6. 配置frame

下图是配置后的Mange Chirps和Mange BPM Chirps的结果图

不知道我哪里出了问题,导致设置为BPM模式下输出的bin文件大小有误,应该是25MB,却变为了50MB.

我已在英文论坛提了相同的问题,望尽快回复,谢谢!