This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM96000: 74h 寄存器中,当我使用高频率的PWM输出(24Khz),依据手册我只能用Mode0获取转速,但是我不是很理解Mode0下 可以获取到的最小Rpm和Pwm频率之间的关系

Part Number: LM96000


我有4个问题

问题1. 按照手册中5F-61h寄存器描述,我可以配置的PWM频率为下图所示

 在74h寄存器中的Pwm频率和5F-61h寄存器中描述的是一个东西吗?

问题2:74h寄存器中Pwm频率的单位是什么呢?

问题3: 我理解的是 当Pwm频率为10.01时,在模式0下,当转速小于841RPM的时候读数可能发生错误,是正确的吗?

问题4: 28-2Fh寄存器中的转速,是否为 '16位转速的值' 小于841的时候转速不准确,还是说需要对 '16位转速的值'  进行公式换算后小于841的时候转速不准确呢,如果需要公式换算,公式是什么呢?

谢谢