On the TIDEP-01012 cascade development board, in TDM mode, one frame has 16 chirps. Why is the SNR particularly high for the chirps in the middle?
On the TIDEP-01012 cascade development board, in TDM mode, one frame has 16 chirps. Why is the SNR particularly high for the chirps in the middle?
你好,
请问你是在暗室对固定角反测试看到的这个现象么?
Thanks,
Chris
你好,
如下配置是一个frame里有12x16个chirp。由于是多片级联,不同芯片会有差异,建议看看单芯片。
Thanks,
Chris
您说的单芯片是改成这样吗?
local start_chirp_tx = 0
local end_chirp_tx = 0
你好,
可以你这样尝试。也可以单片可以修改下面配置,只使能第一个芯片,当然chirp配置也要做相应修改。
RadarDevice = {1, 1, 1, 1} -- {dev1, dev2, dev3, dev4}, 1: Enable, 0: Disable
cascade_mode_list = {1, 2, 2, 2} -- 0: Single chip, 1: Master, 2: Slave
Thanks,
Chris