On the TIDEP-01012 cascade development board, in TDM mode, one frame has 16 chirps. Why is the SNR particularly high for the chirps in the middle?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
On the TIDEP-01012 cascade development board, in TDM mode, one frame has 16 chirps. Why is the SNR particularly high for the chirps in the middle?
你好,
请问你是在暗室对固定角反测试看到的这个现象么?
Thanks,
Chris
你好,
如下配置是一个frame里有12x16个chirp。由于是多片级联,不同芯片会有差异,建议看看单芯片。
Thanks,
Chris
您说的单芯片是改成这样吗?
local start_chirp_tx = 0
local end_chirp_tx = 0
你好,
可以你这样尝试。也可以单片可以修改下面配置,只使能第一个芯片,当然chirp配置也要做相应修改。
RadarDevice = {1, 1, 1, 1} -- {dev1, dev2, dev3, dev4}, 1: Enable, 0: Disable
cascade_mode_list = {1, 2, 2, 2} -- 0: Single chip, 1: Master, 2: Slave
Thanks,
Chris