This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC7201: TDC7201进行激光飞行时间测距时,当采用TDC1测量时间超过最低测量精度12ns时(即用TDC1测量3ns的飞行时间),为何GUI界面会显示140ns的测量结果而不是测不出来?这个140ns的测量结果有参考价值吗?

Part Number: TDC7201


  • 您好

    TDC7201测量结果显示问题解析‌:

    • 测量原理‌:TDC7201通过测量START与STOP脉冲之间的时间(飞行时间,即TOF)来进行测距。内置两个时间数字转换器(TDC),每个TDC可执行秒表功能,测量START脉冲与多达5个STOP脉冲之间的时间间隔。

    • 测量精度与范围‌:TDC7201设计用于测量4厘米到数千米范围内的距离,具有皮秒级精度,非常适合测距应用。

    • 问题解析‌:

      • 当TDC1测量时间超过其最低测量精度12ns时,如测量3ns的飞行时间,理论上应能准确测量。
      • GUI界面显示140ns而非测不出,可能原因包括:测量误差、系统延迟、软件处理错误等。
      • 140ns的测量结果若远超实际飞行时间,则参考价值有限,需进一步排查测量系统的问题。

    综上所述,TDC7201在测量飞行时间时,若GUI界面显示的测量结果远超实际值,该结果可能不具有参考价值,需检查测量系统以确保准确性