This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I used AWR1642+DCA1000 to detect liquids from stationary objects, and the parameters set in mmWaveStudio were as follows: 128 chirp, 1 frame. After receiving the data, the FFT transformation of the data was carried out, and 30 times of detection, and it was found that the amplitude of the corresponding position of the FFT transformation (R-A) graph showed a downward trend in these 30 times, why is this? Later, it was changed to 5 frames, and the result is shown in the figure below, I would like to ask what caused this?
detect liquids from stationary objects
液体是不流动的,例如一个罐子里的水?
如果你要检测类似液位计的功能,建议参考radar toolbox里level sensing的例子。
AWR1642BOOST的天线FOV比较大。
Thanks,
Chris