你好,
1、SN74CBT3257C能否用于通讯信号的选通,其中BMS+对外,CAN与BMS485对内,二选一,选择CAN通讯或者RS485通讯。

2、此芯片可用于双向传输信号?
3、规格书的最大耐压值标的是7V,目前所有端口对GND电压都在规格范围内,但芯片却出现损坏的情况,损坏的具体现象为第3和4脚阻值为20Ω,第5和7脚阻值为50kΩ;另外两组不用的通道阻值也较低(即:第9和11脚、第12和14脚阻值都为50kΩ)。
请帮忙解答一下,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
1、SN74CBT3257C能否用于通讯信号的选通,其中BMS+对外,CAN与BMS485对内,二选一,选择CAN通讯或者RS485通讯。

2、此芯片可用于双向传输信号?
3、规格书的最大耐压值标的是7V,目前所有端口对GND电压都在规格范围内,但芯片却出现损坏的情况,损坏的具体现象为第3和4脚阻值为20Ω,第5和7脚阻值为50kΩ;另外两组不用的通道阻值也较低(即:第9和11脚、第12和14脚阻值都为50kΩ)。
请帮忙解答一下,谢谢!
您好,
支持双向传输。
选择CAN通讯或者RS485通讯
这是标准的协议电平吗? 共模电压是多少?
请参考数据手册“recommended operating conditions” 最高5.5v使用芯片。