This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX8108: 在实际设计中存在输出与切换波形不匹配的问题

Part Number: TMUX8108


在验证TMUX8108的时候发现输出波形与实际切换波形不对应

图一是设计原理图:

VDD供电是30V,VSS供电是-30V,VCC1是15V,VCC2是-15VEN是高电平,A1和A2是低电平,A0在高低电平中切换

图二是抓出的实际波形

绿色是A0信号切换时序,最高为3.3V

黄色是OUT输出波形

问题:这个现象正常吗?为什么在切换的时候会有一个台阶?