This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CB3Q16211: SN74CB3Q16211DGVR pin-to-pin 替代器件

Part Number: SN74CB3Q16211

我们现在设计中使用的型号为SN74CB3Q16211DGVR, 因为这个器件TI已经生产超过15年,请问这个器件的lifecycle是多少?

另外,我在TI网站找到另外一款SN74CBTLV16211VR器件,初步看下来是可以符合我们的设计使用且与SN74CB3Q16211DGVR的symbol和footprint是一样的,请根据我们的设计(如下图)帮我们再看看这两款器件是否可以pin-to-pin替代?

下图设计中,供电电压为3.3V,所有的信号均为3.3V LVCMOS电平,信号速率最高为25MHz