This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX9616N: TMUX9616N 能否通过恒流信号?

Part Number: TMUX9616N

你好,

继之前出现故障情况后更换PCB并插上新的芯片,我们发现好像无法正常开关 S/D

030918ED7CF5E7988B03AE70CC91A7FF.jpg

逻辑电源3.3V,正负高压为正负90V;

所有chn都是on的时候, 控制clr=0或者=1时,控制通道的开关;

source输入的是1ms的+1ma恒流90V以及1ms的-1ma恒流90V;

操作流程是
1. chn=on, clr=1, 给source输入+1ma
2. clr=0, 延时1ms后, clr=1
3. 给source输入-1ma
4. clr=0, 延时1ms后, clr=1
重复以上流程10次

波形图如上