Part Number: MUX509
MUX509芯片手册标明切换时间为92ns。

STM32控制MUX509用作调整增益放大器放大反馈电阻时,采用AD芯片以100Hz的采样率采集放大后的电压,发现放大倍数在切换时是逐渐变化的,且远远大于这个转换时间,需要延时200ms以上,否则放大倍数在切换时会瞬间增大。放大电路如下:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
这个转换时间(Transition Time)是以数字地址信号(A0、A1)上升或下降至50%的电平值为起点,以MUX50x 上升或下降至输出幅值的90%为终点的计时时间,如下图所示,而数字地址信号的识别电平高电平是2.0V min,识别低电平是0.8V max;所以需要实际测量下,在实际控制数字地址信号(A0、A1)发出时至MUX50x 输出达到期望值的时间具体是多少?而不能单纯的将MUX50x 的转换时间92ns作为这个达到信号稳定的延迟时间;
另外,这个转换时间不是固定的,它与供电电压、单/双供电电源、阻性负载、容性负载、温度等有关,92ns是双电源供电,VS = 10 V, RL = 300 Ω, CL= 35 pF时的一个典型值;
导通电阻RON 125Ω 也是VS = 0 V, ICH = 1 mA 时的典型值;