This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MUX509: 切换时间过长

Part Number: MUX509


MUX509芯片手册标明切换时间为92ns。

STM32控制MUX509用作调整增益放大器放大反馈电阻时,采用AD芯片以100Hz的采样率采集放大后的电压,发现放大倍数在切换时是逐渐变化的,且远远大于这个转换时间,需要延时200ms以上,否则放大倍数在切换时会瞬间增大。放大电路如下:

  • 您好,

    这个转换时间(Transition Time)是以数字地址信号(A0、A1)上升或下降至50%的电平值为起点,以MUX50x 上升或下降至输出幅值的90%为终点的计时时间,如下图所示,而数字地址信号的识别电平高电平是2.0V min,识别低电平是0.8V max;所以需要实际测量下,在实际控制数字地址信号(A0、A1)发出时至MUX50x 输出达到期望值的时间具体是多少?而不能单纯的将MUX50x 的转换时间92ns作为这个达到信号稳定的延迟时间;

    另外,这个转换时间不是固定的,它与供电电压、单/双供电电源、阻性负载、容性负载、温度等有关,92ns是双电源供电,VS = 10 V, RL = 300 Ω, CL= 35 pF时的一个典型值;

    导通电阻RON 125Ω 也是VS = 0 V, ICH = 1 mA 时的典型值;

  • 您好,

    非常感谢您有价值的回复!

    我觉得实测转换时间与标称相差太大,是ns级别和ms级别的差别,另附一张测试图,黄色为开关电平,蓝色为选通电压变化,可见经历了10ms以上的时间电压才基本切换到选通通道电压,这是否与92ns的转换时间相差甚大(如果选通时间在1ms以下还可以理解)?选通时间过长对我的设计十分不利,想请教一下是否有硬件上减小切换时间的方法?谢谢

  • 首先,我需要先向您确认一下,

    1、上面示波器图中,蓝色信号线为A0、A1通道选择地址信号吗?黄色信号线为MUX50x 开关输出信号吗?

    2、蓝色信号A0、A1的电平幅值是多少?仅从您截图看,每格0.5V,不到3个格,即电平不到1.5V,而MUX50x 的逻辑电平需达到2V min才能被认为是高电平