This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3A24157: 可承受电压

Part Number: TS3A24157


如果我在ts3a24157的COM1通道输入大约10mA电流,电流通过NC1开关流向负载(约6kΩ),再由NC2流至COM2,COM2接地,那么COM1处电压大约有60V。ts3a能够承受这个电压吗,还是说输入电压不得高于VCC。

我之前看其他人用过这款单刀双掷芯片,输入COM的电压有15V,但不清楚他是否成功,数据手册上又好像是不允许输入这么高的电压。

如果这款芯片不能实现这样的功能,那能推荐一下其他合适的高压单刀双掷芯片吗?