Part Number: TS5A23159
There are two IIC controllers in the project, which need to time-share control the devices hung on the IIC bus, and the IIC rate is 1MHz. I want to know whether the TS5A23159 can be used as the I2C switcher

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TS5A23159
There are two IIC controllers in the project, which need to time-share control the devices hung on the IIC bus, and the IIC rate is 1MHz. I want to know whether the TS5A23159 can be used as the I2C switcher