There are two IIC controllers in the project, which need to time-share control the devices hung on the IIC bus, and the IIC rate is 1MHz. I want to know whether the TS5A23159 can be used as the I2C switcher

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There are two IIC controllers in the project, which need to time-share control the devices hung on the IIC bus, and the IIC rate is 1MHz. I want to know whether the TS5A23159 can be used as the I2C switcher