This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MUX506: 输入的波形通过多路复用时,信号质量会发生变化吗?Datasheet没有描述信号输入输出前后的质量

Part Number: MUX506


应用场景如下:

1. 输入信号波形如下:

VIH/VIL: -1.5-+4.5V

VO: -1.5~+4.5v, Only one strobe level,edge strobe

VTvoltage:-1.5~+4.5v level by pin
Driver Source Resistance:50Ω(±1.5Ω)

Tr: 350 ps(VIH = 1.6 V, VIL = 0.4 V)   2v的20%~80%时的rise time

Tf:350 ps(VIH =1.6 V,VIL= 0.4 V)  2v的20%~80%时的fall time

2. 如上信号通过MUX506后,波形质量会失真吗?

3. 若MUX506不满足要求,有其他推荐的型号满足信号质量不失真吗?通道数越多越好。

4. 若有Demo板能否测试一下信号质量波形?