This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4052B: 在3.3V供电时的VIL和VIH多少呢?

Part Number: CD4052B
Other Parts Discussed in Thread: TMUX1109, TMUX1209

您好:

我们仪器里用到了CD4052器件,以前的供电为+5V/-6V,我重新修改该电路板,想去掉负电源。

我刚看了手册,理解着,该器件的供电对数字电平和输入电压是不一样的。+5V/-6V的时候,输入电压可以在-6V~+5V之间。逻辑电平还是按照5V/0。是这样吗?

1、我们的MCU是3.3V供电,多路复用开关输入电压也不会超过3.3V。那么我是否可以改成3.3V/0供电呢??看了手册是有一个这样的典型应用的,应该是没问题把。

2、手册里面只提供了5V/10V/15V三个电压的VIL和VIH,3.3V的高低电平对应多少没有说,咱们能否提供一下呢?或者我按照上图的典型电路(MCU和多路复用器都是3.3V)去接,逻辑电平能够匹配把。

非常感谢!

  • 您好,

             CD4052B在3.3V供电下可以工作。

              但由于CD4000系列芯片主要是为高压应用的,在低压供电时导通阻抗较大,因此无法保证在3.3V供电情况下的芯片性能。

             因此对于3.3V信号的切换,建议评估一下低压的芯片如TMUX1109 或者TMUX1209。 

  • 好的,感谢您的回复。

    1、您说的,它的导通阻抗大,指的是多路复用开关导通阻抗大是吧,我后端接的是仪表放大器,高阻输入,所以即使阻抗大也没啥影响把?

    2、3.3V时候的VIL和VIH大概是多少呢,我看了手册,5V时候的VIH为3.5V,headroom为1.5V。VIL=0.8V。那么3.3V供电时候VIL不变,VIH=1.8V吗?

    3、我搭建电路实测过了,可以用。