已官网的图片为例,PORT1是主函数,里面有TA1和TA2两个子函数,
对于Inclusive Size:
| PORT1 | 32 |
| TA1 | 8 |
| TA2 | 8 |
我的疑问是:如果TA1和TA2在PORT1里面为if(){TA1}else{TA2},结构,是不是就不用管PORT1用了多少,反正程序每次只会进TA1和TA2中的一个,PORT1哪怕100%也不会有什么影响?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
已官网的图片为例,PORT1是主函数,里面有TA1和TA2两个子函数,
对于Inclusive Size:
| PORT1 | 32 |
| TA1 | 8 |
| TA2 | 8 |
我的疑问是:如果TA1和TA2在PORT1里面为if(){TA1}else{TA2},结构,是不是就不用管PORT1用了多少,反正程序每次只会进TA1和TA2中的一个,PORT1哪怕100%也不会有什么影响?
您好,Port1 的异步大小 (函数使用的堆栈,不包括子函数使用的内容) 为 24。由于 inclusive size总计为32,因此只会为被调用的子函数留出8。