• CODECOMPOSER: 如何在CCS中的target configuration中设置同时连接两块awr1843

    Part Number: CODECOMPOSER
    Other Parts Discussed in Thread: AWR1843

    在高级设置里面选择添加两块awr1843之后,还需要设置其他的参数吗?

    在启动如上图所示的连接配置文件后,选中其中一个awr1843的芯片进行“connect target”后出现了如下的报错,这该怎么解决呢?

    CS_DAP_0: Error connecting to the target: (Error -1170 @ 0x0) Unable…

  • AWR1843: CCS 溢出检测使用问题(dynamic stack overflow checking)

    Part Number: AWR1843

    在MSS工程编译中开启溢出检测选项,提示在引用的lib库中未定义handle_stkovf,且__stack地址与启动入口地址_c_int00均报重定义错误,与MSS工程中自定义boot.asm中的地址冲突。

    handle_stkovf这一地址应当如何配置?在AWR1843的相关文档中没有找到对应的结果,有无可以参考的例程或文档?

  • CCS编译报错,gmake和gmake[1],怎么解决?看不懂

    Other Parts Discussed in Thread: AWR1843

    CCS10.1.0+mmwave SDK 3.5版本,进行AWR1843毫米波雷达开发。

    程序编译出错,截图如下。

    xdctools_core中有相关文件,但是不知道什么意思。这个报错,needed by‘BIOS.obj’是什么意思,

    怎么解决?与什么配置或改动有关?

  • CCS编译报错,gmake和gmake[1],怎么解决?看不懂

    Other Parts Discussed in Thread: AWR1843

    CCS10.1.0+mmwave SDK 3.5版本,进行AWR1843毫米波雷达开发。

    程序编译出错,截图如下。

    xdctools_core中有相关文件,但是不知道什么意思。这个报错,needed by‘BIOS.obj’是什么意思,

    怎么解决?与什么配置或改动有关?

  • CCS编译出错,#10008-D cannot find file,怎么解决。

    Other Parts Discussed in Thread: AWR1843

    Win10,64位平台电脑。

    CCS版本10.1.0,mmwave SDK软件为3.5.0.4版本。做AWR1843毫米波雷达开发,编译dss报错#10008-D如下,这是什么原因,查了网上资料,说是按照图2修改,怎么修改?这个图中标亮的例子填的对不对?

  • CCS10.1.0新建CCS工程后,还未进行任何配置或操作,编译dss和mss时都报错,dss报错是:warning#10247-D:creating output section “.text”without a SECTIONS specification以及error #10234-D:unresolved symbols remain和error #10010:during linking;.out文件not built等错误,怎么解决?

    Other Parts Discussed in Thread: AWR1843, SYSBIOS

    平台:64位Windows系统。

    安装的CCS版本为10.1.0

    安装的mmwave SDK软件版本为mmwave_sdk_03_04_00_03。

     

    进行毫米波雷达工程的创建(目标板为AWR1843),新建CCS工程中,命名MCU(Cortex R4F架构)对应文件名为m0329_mss,命名DSP(型号为TMS320C674x)对应文件名为m0329_dss。CCS工程新建完成后(过程没有问题,SYS…