SYSCONFIG: CCS12.8的sysconfig报错:Unable to initialize the browser engine.

Part Number: SYSCONFIG
Other Parts Discussed in Thread: C2000WARE

安装好CCS12.8、C2000Ware6.0.0.00以及sysconfig1.24后,从C2000Ware中打开样例的sysconfig文件报错,错误原文为:
Unexpected error encountered when opening the file!  Please make sure the file is within the context of a valid and opened CCS Project.  If the project has errors, these may be preventing this file from opening. 
java.lang.RuntimeException: Unable to initialize the browser engine. For Linux host, please check the dependencies are installed by running the 'ldd' command for the libraries in this folder E:\CCS12.8\ccs\eclipse\configuration\.jxbrowser.bin\7.29.
image.png