Part Number: DRV8263S-Q1EVM
Other Parts Discussed in Thread: DRV8263-Q1
After applying 48V to the DRV8263-Q1 evaluation board, I smelled a bit of burning, so I changed the voltage to 12V, but I only measured 0.02V on the board. I checked the fuse, it's fine(It shows continuity when tested with a multimeter). Why can't this board handle 48V, and what should I do next to get it running again?