This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PSPICE-FOR-TI: Source part使用FileStim8, description : Digital Stimulus (From File)

Part Number: PSPICE-FOR-TI


請問Source part使用FileStim8, file的格式為何?

我使用Source part使用FileStim1 格式如下是正確的, 但FileStim8不知道應該怎麼編輯?

DTx

0ms 1
10ms 0
20ms 1
30ms 0
40ms 1

感謝解惑!