Part Number: PSPICE-FOR-TI
請問Source part使用FileStim8, file的格式為何?
我使用Source part使用FileStim1 格式如下是正確的, 但FileStim8不知道應該怎麼編輯?
DTx
0ms 1
10ms 0
20ms 1
30ms 0
40ms 1
感謝解惑!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PSPICE-FOR-TI
請問Source part使用FileStim8, file的格式為何?
我使用Source part使用FileStim1 格式如下是正確的, 但FileStim8不知道應該怎麼編輯?
DTx
0ms 1
10ms 0
20ms 1
30ms 0
40ms 1
感謝解惑!
为更加有效地解决您的问题,我将您的问题发布在了E2E英文技术论坛上,如下链接,E2E英文论坛工程师让看下help文件,给出如下截图,您看下是否有帮助?

E2E英文论坛工程师又给出如下回复,看下是否解决了您的疑问:
The user needs to have a bus connected to the symbol with the correct alias. In this example, the net alias for the bus is DATA[0:7] which will be expanded by the software to the individual wires DATA0 to DATA7:
您需要使用正确的别名将总线连接到符号。在此示例中,总线的网络别名是DATA[0:7] ,软件将其扩展为单独的信号线DATA0至DATA7:

stm文件内容:
DATA0 DATA1 DATA2 DATA3 DATA4 DATA5 DATA6 DATA7
0ns 00000000
1us 00000001
2us 00000010
3us 00000100
4us 00010000
5us 00100000
6us 01000000
7us 10000000
8us 00000011
20ms 00000111
21ms 00001001
36ms 00010001
37ms 00110001
47ms 11000001
48ms 11100001
56ms 00001111
57ms 00111111
64ms 11110001
65ms 11111111
您试下下面project是否可以运行?