This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PSPICEFORTI 出现一大推错误,是模型 的问题还是哪的问题,有办法解决吗?

X_U11.Isupply VCC_BAR 0 7.8E-3
X_U11.EVSx X_U11.VSx 0 VCC_BAR 0 1
X_U11.V10 X_U11.N019 0 79.3
X_U11.V11 0 X_U11.N014 19.3
X_U11.D10 X_U11.N014 N49301 X_U11.D
X_U11.D12 N49301 X_U11.N019 X_U11.D
X_U11.D13 X_U11.N014 N49414 X_U11.D
X_U11.D14 N49414 X_U11.N019 X_U11.D
X_U11.D15 X_U11.N022 N49301 X_U11.Ddiff
X_U11.D16 X_U11.N023 N49414 X_U11.Ddiff
X_U11.D17 X_U11.N022 N49414 X_U11.D
X_U11.D18 X_U11.N023 N49301 X_U11.D
X_U11.D19 X_U11.N026 X_U11.N028 X_U11.D
X_U11.D20 X_U11.N026 N49301 X_U11.D
X_U11.D1 X_U11.N029 X_U11.N027 X_U11.D
X_U11.V4 X_U11.N029 0 1.5
X_U11.D2 N49301 X_U11.N027 X_U11.D
X_U11.D3 X_U11.N004 X_U11.N006 X_U11.D
X_U11.D4 N49414 X_U11.N006 X_U11.D
X_U11.V5 X_U11.N004 0 1.5
X_U11.BIbiasP X_U11.N027 0 X_U11.I X_U11.IF V
--------------------------------------------$
ERROR(ORPSIM-16147): Invalid parameter
+ 3 0 0 V 7 0 0 0e-6 104e-6
X_U11.BIbiasN X_U11.N006 0 X_U11.I X_U11.IF V
--------------------------------------------$
ERROR(ORPSIM-16147): Invalid parameter
+ 3 0 0 V 7 0 0 0e-6 104e-6
X_U11.G1 0 X_U11.NNN N49414 0 1
X_U11.G2 0 X_U11.PPP N49301 0 1
X_U11.R2 X_U11.NNN 0 1
X_U11.R5 X_U11.PPP 0 1
X_U11.EINN X_U11.VSL_INN 0 X_U11.NNN 0 1
X_U11.EINP X_U11.VSL_INP 0 X_U11.PPP 0 1
X_U11.DCL1 X_U11.NCL1 X_U11.NNN X_U11.D
X_U11.DCL2 X_U11.NNN X_U11.NCL2 X_U11.D
X_U11.VCL3 X_U11.NCL1 X_U11.NCL3 1.5
X_U11.VCL4 X_U11.NCL4 X_U11.NCL2 1.5
X_U11.VCL2 X_U11.NCL3 0 -2
X_U11.VCL1 X_U11.NCL4 0 70
X_U11.DCL3 X_U11.NCL6 X_U11.PPP X_U11.D
X_U11.DCL4 X_U11.PPP X_U11.NCL5 X_U11.D
X_U11.VCL5 X_U11.NCL6 X_U11.NCL3 1.5
X_U11.VCL6 X_U11.NCL4 X_U11.NCL5 1.5
X_U11.Vos X_U11.N009 X_U11.N008 0E-6
X_U11.RCM_INN X_U11.N010 X_U11.N009 12000.165
X_U11.RCM_INP X_U11.INPx X_U11.VSL_OUTP 12000.0
X_U11.LCM_INN X_U11.N010 X_U11.INNx 0.0317E-3
X_U11.BSL1 0 X_U11.VSL_OUTP X_U11.I X_U11.limit 1*V VSL_INP
----------------------------------------------------$
ERROR(ORPSIM-16147): Invalid parameter
+ VSL_OUTP 0.4 -0.4
X_U11.C4 X_U11.VSL_OUTP 0 1E-15
X_U11.R10 X_U11.VSL_OUTP 0 10E9
X_U11.R_INN_OUT X_U11.OUTx X_U11.INNx 600E3
X_U11.R1 0 X_U11.OUTx 1E12
X_U11.R_INP_REF1 X_U11.INPx X_U11.REFMID 569988.7
X_U11.R_REF1 VCC_BAR X_U11.REFMID 60E3
X_U11.R_REF2 0 X_U11.REFMID 60E3
X_U11.R3 N49414 0 562E3
X_U11.R4 0 N49301 562E3
X_U11.D9 X_U11.N018 X_U11.N017 X_U11.DN
X_U11.D11 X_U11.N016 X_U11.N015 X_U11.DN
X_U11.H1 X_U11.N011 X_U11.OUTx X_U11.Vn1 707.1067812
X_U11.Vn1 X_U11.N015 0 0
X_U11.Vn2 X_U11.N016 0 0.65
X_U11.Vn3 X_U11.N017 0 0
X_U11.Vn4 X_U11.N018 0 0.65
X_U11.H2 X_U11.N011 X_U11.VX X_U11.Vn3 707.1067812
X_U11.BSL2 0 X_U11.VY X_U11.I X_U11.limit 1*V VX
----------------------------------------------$
ERROR(ORPSIM-16147): Invalid parameter
+ VY 0.0085 -0.0086
X_U11.C3 X_U11.VY 0 1E-9
X_U11.R11 X_U11.VY 0 1E9
X_U11.R6 X_U11.VZ 0 100E9
X_U11.G3 0 X_U11.VZ X_U11.VY X_U11.VO 0.3
X_U11.C1 X_U11.VZ 0 0.61E-9
X_U11.G4 0 X_U11.VO X_U11.VZ 0 7m
X_U11.R7 X_U11.VO 0 5
X_U11.C2 X_U11.VO 0 20n
X_U11.D5 X_U11.N020 X_U11.VZ X_U11.D
X_U11.D6 X_U11.VZ X_U11.N021 X_U11.D
X_U11.V6 0 X_U11.N020 150
X_U11.V7 0 X_U11.N021 -150
X_U11.V12 X_U11.N028 0 -5
X_U11.R8 X_U11.N026 0 40E3
X_U11.D21 X_U11.N005 X_U11.N003 X_U11.D
X_U11.D22 X_U11.N005 N49414 X_U11.D
X_U11.V13 X_U11.N003 0 -5
X_U11.R9 0 X_U11.N005 40E3
X_U11.G5 0 X_U11.OUTx X_U11.INPx X_U11.INNx 100
X_U11.Rout X_U11.VVO VOUT3 0.2 Noiseless
-------------------------------$
ERROR(ORPSIM-16015): Unknown parameter.
X_U11.Eout X_U11.VVO 0 X_U11.VO 0 1
X_U11.C5 X_U11.N032 X_U11.N031 {C1a_PSRR}
X_U11.G6 0 X_U11.N031 X_U11.VSx 0 {G1_PSRR}
X_U11.R12 X_U11.N031 0 1 Noiseless
-------------------------$
ERROR(ORPSIM-16015): Unknown parameter.
X_U11.R13 X_U11.N032 X_U11.N031 {R1a_PSRR} Noiseless
-------------------------------------------$
ERROR(ORPSIM-16015): Unknown parameter.
X_U11.R14 X_U11.N032 0 {R2a_PSRR} Noiseless
----------------------------------$
ERROR(ORPSIM-16015): Unknown parameter.
X_U11.C6 X_U11.N034 X_U11.N033 {C1b_PSRR}
X_U11.R15 X_U11.N034 0 {R2b_PSRR} Noiseless
----------------------------------$
ERROR(ORPSIM-16015): Unknown parameter.
X_U11.R16 X_U11.N034 X_U11.N033 {R1b_PSRR} Noiseless
-------------------------------------------$
ERROR(ORPSIM-16015): Unknown parameter.
X_U11.G7 0 X_U11.N033 X_U11.N032 0 1
X_U11.R17 X_U11.N033 0 1 Noiseless
-------------------------$
ERROR(ORPSIM-16015): Unknown parameter.
X_U11.G8 0 X_U11.PSRR X_U11.N034 0 {G2_PSRR}
X_U11.R18 X_U11.PSRR 0 1 Noiseless
-------------------------$
ERROR(ORPSIM-16015): Unknown parameter.
X_U11.G9 X_U11.VSL_INN X_U11.N008 X_U11.PSRR 0 1k
X_U11.R19 X_U11.N008 X_U11.VSL_INN 1m
X_U11.B1 X_U11.Satp X_U11.VSx X_U11.I X_U11.1m*Dnlim Ap
-----------------------------------------------------$
ERROR(ORPSIM-16147): Invalid parameter
+ + Bp*V Vimon 2 +Cp*V Vimon 2 **2 Ap 1m
X_U11.R20 X_U11.Satp X_U11.VSx 1k
X_U11.C7 X_U11.Satp X_U11.VSx 1n
X_U11.B2 0 X_U11.Satn X_U11.I X_U11.1m*Dnlim Mn*
---------------------------------------------$
ERROR(ORPSIM-16147): Invalid parameter
+ -V Vimon 2 +OSn OSn 1m
X_U11.R21 X_U11.Satn 0 1k
X_U11.C8 X_U11.Satn 0 1n
X_U11.B3 0 X_U11.Vimon X_U11.I X_U11.1m*I Rout
------------------------------------------$
ERROR(ORPSIM-16147): Invalid parameter
X_U11.G11 0 X_U11.Vsatn X_U11.Satn 0 1k
X_U11.R23 X_U11.Vsatn 0 1m
X_U11.C9 X_U11.Vsatp 0 1n
X_U11.C10 X_U11.Vsatn 0 1n
X_U11.DOP X_U11.Vsatp X_U11.VO X_U11.DO
X_U11.DON X_U11.VO X_U11.Vsatn X_U11.DO
X_U11.C11 X_U11.VO X_U11.Vsatp 1f
X_U11.C12 X_U11.VO X_U11.Vsatn 1f
.model X_U11.D D IS 1E-14
.model X_U11.DN D IS 3.9E-11 KF 2.4E-16
.model X_U11.Ddiff D IS 1e-14 BV 19.3
.param gain_PSRR {pow(10, (-Rej_dc_PSRR/20))}
.param C1a_PSRR {1 / (2 * pi * R1a_PSRR * fz1_PSRR)}
.param R2a_PSRR {R1a_PSRR/ ((2 * pi * fp1_PSRR * C1a_PSRR* R1a_PSRR)- 1)}
.param actual1_PSRR {R2a_PSRR / (R1a_PSRR + R2a_PSRR)}
.param G1_PSRR {gain_PSRR/actual1_PSRR}
.param Rej_dc_PSRR 120
.param R1a_PSRR 100k
.param fz1_PSRR 2.5k
.param fp1_PSRR 50Meg
.param C1b_PSRR {1 / (2 * pi * R1b_PSRR * fz2_PSRR)}
.param R2b_PSRR {R1b_PSRR/ ((2 * pi * fp2_PSRR * C1b_PSRR* R1b_PSRR)- 1)}
.param actual2_PSRR {R2b_PSRR / (R1b_PSRR + R2b_PSRR)}
.param G2_PSRR {1/actual2_PSRR}
.param R1b_PSRR 100k
.param fz2_PSRR 310k
.param fp2_PSRR {fp1_PSRR}
.model X_U11.DO D Vfwd
------------------$
ERROR -- 'Vfwd' is not a model parameter name


ERROR(ORPSIM-15113): Model IF used by X_U11.BIbiasP is undefined

ERROR(ORPSIM-15113): Model IF used by X_U11.BIbiasN is undefined

ERROR(ORPSIM-15113): Model limit used by X_U11.BSL1 is undefined

ERROR(ORPSIM-15113): Model limit used by X_U11.BSL2 is undefined

ERROR(ORPSIM-15113): Model 1m*Dnlim used by X_U11.B1 is undefined

ERROR(ORPSIM-15113): Model 1m*Dnlim used by X_U11.B2 is undefined

ERROR(ORPSIM-15113): Model 1m*I used by X_U11.B3 is undefined