Part Number: PSPICE-FOR-TI

并且该目录下没有日志文件,跟论坛上出现过的一样。另外,电脑系统位window10
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工程师回复如下:
Our team member shared a way to solve the installation issue. It is because Endpoint Protector was blocking the installer from running and this issue was fixed by adding to the 'Allow' list' and updating local policies. I solve this by updating my local policies by right clicking on the Endpoint Protector icon (the one that looks like a traffic light) in the system tray and selecting "Update Policies Now".
解决方法是:
通过右键单击系统托盘中的Endpoint Protector图标(看起来像交通灯的图标)并选择"Update Policies Now"来更新我的本地策略来解决此问题。
您试下是否可以解决问题?

design tools 工程师最新回复如下,您尝试下看是否可以解决问题:
请您尝试对系统进行以下更新:
系统策略阻止执行安装程序使用的算法。
A) 打开Windows控制面板->管理工具->本地安全策略
(B) 在左列中,选择本地策略->安全选项
(c) 在右侧列中,选择系统加密:使用符合FIPS的算法进行加密,散列和签名。 双击此选项并将其设置为禁用(如果已启用)。
(d) 重新启动计算机并再次执行安装
Please have the customer try this following updates to their system:
System policies are preventing execution of the algorithm used by installer.
a). Open Windows Control Panel->Administrative tools->Local Security Policy
(b). On the left hand side column, select Local Policies->Security Options
(c). On the right hand side column, select System Cryptography: Use FIPS compliant algorithms for encryption, hashing and signing. Double click on this and set it to disabled if it is enabled.
(d). Restart the machine and perform installation again