This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
波形看起来正常,只是LM318的供电电压范围+-5V~+-20V,所以+-3V供电是不允许的。
另外,我看您电路+-3V供电,输入也是3V幅值,所以看起来是削波的,LM318 不是轨至轨输入,比如+-15V供电,输入电压范围最小+-11.5V,所以和供电电压有3.5V的headroom。
最近我看您使用运放搭建电路或者滤波器的例子很多,我建议您可以尝试使用TINA,不论是DC传输特性,还是AC传输特性,以及瞬态响应的仿真都比较方便。