This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位前辈好!
我就想用btool看一下connection setting,
但是我尝试用BT00l去看cc2540的connection setting发现都是一样的,而且和我的设定也不一样。我的设定如下
// Minimum connection interval (units of 1.25ms, 80=100ms) if automatic parameter update request is enabled
#define DEFAULT_DESIRED_MIN_CONN_INTERVAL 20
// Maximum connection interval (units of 1.25ms, 800=1000ms) if automatic parameter update request is enabled
#define DEFAULT_DESIRED_MAX_CONN_INTERVAL 20
// Slave latency to use if automatic parameter update request is enabled
#define DEFAULT_DESIRED_SLAVE_LATENCY 0
// Supervision timeout value (units of 10ms, 1000=10s) if automatic parameter update request is enabled
#define DEFAULT_DESIRED_CONN_TIMEOUT 500
// Whether to enable automatic parameter update request when a connection is formed
#define DEFAULT_ENABLE_UPDATE_REQUEST TRUE
我尝试的去改#define DEFAULT_DESIRED_MAX_CONN_INTERVAL,btool的显示也没有任何变化.
难道btool里面的这个connection setting不是我设备的设定吗?请高手给指点一下,谢谢!
你好!
我用的是simpleBLEPeripheral这个工程,改动了一点,我的疑问是btool抓的connection setting和我的初始化设定不一样,我的工程里面没有动态的改变connection setting.
GAPRole_SetParameter( GAPROLE_PARAM_UPDATE_ENABLE, sizeof( uint8 ), &enable_update_request );
你好,
Update_Para的说明在peripheral.c函数里面
static uint8_t gapRole_ParamUpdateEnable = FALSE;
// Check whether update parameter request is enabled
if (gapRole_ParamUpdateEnable == TRUE)
{
// Get the minimum time upon connection establishment before the
// peripheral can start a connection update procedure.
uint16_t timeout = GAP_GetParamValue(TGAP_CONN_PAUSE_PERIPHERAL);
Util_restartClock(&startUpdateClock, timeout*1000);
}
你需要把定义改为TRUE
你好!
谢谢你的回复。
我看了一下,我的定义是static uint8 gapRole_ParamUpdateEnable = FALSE;
你好,
建议你把下面的数值加大后尝试
// Minimum connection interval (units of 1.25ms, 80=100ms) if automatic parameter update request is enabled
#define DEFAULT_DESIRED_MIN_CONN_INTERVAL 20
// Maximum connection interval (units of 1.25ms, 800=1000ms) if automatic parameter update request is enabled
#define DEFAULT_DESIRED_MAX_CONN_INTERVAL 20
下午我在 实验室也测试一下然后再反馈你。
你好,
Update_Para的说明在peripheral.c函数里面
static uint8_t gapRole_ParamUpdateEnable = FALSE;
// Check whether update parameter request is enabled
if (gapRole_ParamUpdateEnable == TRUE)
{
// Get the minimum time upon connection establishment before the
// peripheral can start a connection update procedure.
uint16_t timeout = GAP_GetParamValue(TGAP_CONN_PAUSE_PERIPHERAL);
Util_restartClock(&startUpdateClock, timeout*1000);
}
你需要把定义改为TRUE