This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2745R10-Q1: channel sounding信道探测扩展调试数据 是否提供频率差

Part Number: CC2745R10-Q1
Other Parts Discussed in Thread: CC2745P10-Q1

您好,我选用的sdk是最新的channel sounding推出的simplelink_lowpower_f3_sdk_9_12_00_19 ,采用的开发板是LP-EM-CC2745R10-Q1,我在设置

def cs_proc_enable(
car_node,
repeat=0,
wait_for_remote=True,
wait_for_distance=True,
extended_results=True,
wait_for_raw_events=False,
):
    extended_results=True,后会出现local和remote设备的IQ数据以及TQI数据,我现在可以通过这些IQ数据获得相位,并进一步获得这两个设备之间的相位差,但是我有以下问题:

1.如果我才用TI官方提供的PBR测距公式 ,,该公式需要知道频率差和相位差,现在 extended_results可以输出IQ数据并可以得到相位数据,那么频率差我该从上面地方得到呢?
2.如果我在上述代码中选择wait_for_raw_events=True,会得到未经过滤的data,在每一组的local和remote设备中都会出现  requency_compensation这一个参数,请问这个参数是什么意思?
3.我在extended_results结果中,发现了 zh这样的代码,里面的num_steps=75是进行了75次测量,我请问这里的测量的信道是哪一个信道,就是每一次测量蓝牙是在哪一个频段进行工作的?
烦请告知,谢谢