CC256XCQFN-EM: LinuxSPPM和LinuxDEVM是否支持获取CC256XCQFN-EM模块的蓝牙收发状态

Part Number: CC256XCQFN-EM
Other Parts Discussed in Thread: CC2564C

Hello TI Technical Support Team,
 
I am encountering an issue while using the CC256XCQFN-EM module. I would like to inquire whether LinuxSPPM and LinuxDEVM support retrieving the Bluetooth transmit/receive status information of the CC256XCQFN-EM module. I need to obtain the transmit/receive status of the Bluetooth module to enable other chips accordingly.
 
If these two components do not support retrieving the transmit/receive status, could you please advise if there are alternative methods to determine the transmit/receive status of the CC256XCQFN-EM module or the CC2564C chip?
 
Thank you!



TI技术支持团队你好,

我在使用CC256XCQFN-EM模块时遇到了问题,想询问一下LinuxSPPM和LinuxDEVM是否支持获取CC256XCQFN-EM模块的蓝牙收发状态信息,我需要获取蓝牙模块的收发状态以便于给其它芯片进行使能。如果这两个组件不支持获取收发状态,是否有其它方法可以知道CC256XCQFN-EM模块或者CC2564C芯片的收发状态。

感谢!