This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Flash Programmer 2无法识别芯片,但IAR却可以仿真,可能是原因是什么?

问题描述:

  自己做的板子,引出了VDDR,GND,RESET,JTAG_TMS,JTAG_TCK,这五个口做为程序下载及仿真口,如图1所示:

 

 图1 下载测试点

 芯片用的是CC2640-7*7封装,可以用IAR7.70版本仿真,仿真器用的是XDS110-V3,IAR中仿真器的设置如下图所示:

 

 图2 IAR中仿真器的设置

 但是用Flash Programmer 2无法识别芯片,也无法下载程序,现象如下图所示:

 

 图3 Flash Programmer 2中无法识别芯片

 

 图4 如果点击unkown,则弹出如下对话框

 各位坛友是否有遇到类似的情况,请问是什么原因导致的?

 我用Demo板测试,发现,用两线是可以用Flash Programmer 2下载的,那么,我设计的板子是不是哪里没注意到,请大家帮忙找一下原因?

 也请TI的FAE帮帮忙,谢谢!

 注:图中J8是VDDS非VDDR,截图时标注错误