This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All
[目的]
我希望當pc dongle連上cc2640 simpleBLEPeripheral時,pc dongle下cmd向cc2640取得cc2640的rssi。
[Issue]
當我執行GAPRole_SetParameter(GAPROLE_RSSI_READ_RATE, sizeof(uint16_t), &rssi);
<peripheral.c>的gapRole_processStackMsg()的HCI_GAP_EVENT_EVENT不會被通知
[Code]
<simpleBLEPerpheral.c>
static void SimpleBLEPeripheral_taskFxn(UArg a0, UArg a1) { .... Uint16_t rssiReadRate = 3000; GAPRole_SetParameter(GAPROLE_RSSI_READ_RATE, sizeof(uint16_t), &rssiReadRate); ....
}
<peripheral.c>
bStatus_t GAPRole_SetParameter(uint16_t param, uint8_t len, void *pValue) { ………… case GAPROLE_RSSI_READ_RATE: if (len == sizeof(uint16_t)) { gapRole_RSSIReadRate = *((uint16_t*)pValue); if((gapRole_RSSIReadRate) && (gapRole_state == GAPROLE_CONNECTED)) { Util_restartClock(&rssiReadClock, gapRole_RSSIReadRate); } } else { ret = bleInvalidRange; } break; ………… } Static void gapRole_init(void) { GAP_RegisterForMsgs(selfEntity); Util_constructClock(&rssiReadClock, gapRole_clockHandler, 0, 0, false, RSSI_READ_EVT); } Static void gapRole_taskFxn(Uarg a0, Uarg a1) { ……… if (events & RSSI_READ_EVT) { events &= ~RSSI_READ_EVT; // Only get RSSI when in a connection if ((gapRole_state == GAPROLE_CONNECTED) || (gapRole_state == GAPROLE_CONNECTED_ADV)) { // Ask for RSSI hciStatus_t status = NULL; status = HCI_ReadRssiCmd(gapRole_ConnectionHandle); <======== return success // Setup the next event if (gapRole_RSSIReadRate && !status) { Util_restartClock(&rssiReadClock, gapRole_RSSIReadRate); } } } } static void gapRole_processStackMsg(ICall_Hdr *pMsg) { Switch (pMsg->event) { Case HCI_GAP_EVENT_EVENT: <============ Never coming if (pMsg->status == HCI_COMMAND_COMPLETE_EVENT_CODE) { hciEvt_CmdComplete_t* pPkt = (hciEvt_CmdComplete_t*)pMsg; if(pPkt->cmdOpcode == HCI_READ_RSSI) { int8_t rssi = (int8_t)pPkt->pReturnParam[3]; if(((gapRole_state == GAPROLE_CONNECTED) || (gapRole_state == GAPROLE_CONNECTED_ADV)) && (rssi != RSSI_NOT_AVAILABLE)) { // Report RSSI to app if(pGapRoles_AppCGs && pGapRoles_AppCGs->pfnRssiRead) { pGapRoles_AppCGs->pfnRssiRead(rssi); } } } } Break; } }
<peripheral.h>
typedef void (*gapRolesRssiRead_t)(int8_t newRSSI); typedef struct { gapRolesStateNotify_t pfnStateChange; gapRolesRssiRead_t pfnRssiRead; } gapRolesCBs_t;