This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CR2032并联使用问题



大家好 

由于电池容量和空间限制 我们的BLE系统里面用了2颗CR2032并联供电

请问两个颗CR2032直接并联使用会有问题吗?比如两颗电池电压不完全一样造成互相充电(逆电流)等,会存在这样的问题吗?

如果有上述问题,我想这样处理一下:

在通道上加上三极管或者mos

没有用二极管是因为即便是肖特基二极管,导通压降对于CR2032也还是偏大,目前找到了一个VCE最大0.015V的三极管。