If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
因此手册上没有给出单次的具体值,不过总的吞吐量是:When the SPI is configured as SPI slave, the maximum bit rate is 4MHz. When the SPI is configured as SPI master, the maximum bit rate is 12MHz.