This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F的SPI单次的接收,最多可接收多少字节的数据?

Other Parts Discussed in Thread: CC2640R2F

CC2640R2F的SPI单次的接收,最多可接收多少字节的数据?

  • SPI是一种事实标准,并没有一个官方标准,具体到产品中SPI的速率主要看主从器件SPI控制器的性能限制。SPI最大传输速率受以下几个条件影响:
    SPI的最大时钟频率
    CPU处理SPI数据的能力
    输出端驱动能力(PCB所允许的最大信号传输速率)

    因此手册上没有给出单次的具体值,不过总的吞吐量是:When the SPI is configured as SPI slave, the maximum bit rate is 4MHz. When the SPI is configured as SPI master, the maximum bit rate is 12MHz.
  • CC2640R2F 的SPI的最大时钟频率、CPU处理SPI数据的能力、输出端驱动能力(PCB所允许的最大信号传输速率)
    是怎样的?