This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650打开SPI 的时候,程序直接返回NULL,在选择片选管脚的时候报错

SPI_Handle ***(SPI_Handle handle, SPI_Params *params)
{
/* Use union to save on stack allocation */
union {
Semaphore_Params semParams;
Hwi_Params hwiParams;
Swi_Params swiParams;
} paramsUnion;
*** *object;
*** const *hwAttrs;
unsigned int key;

/* Get the pointer to the object and hwAttrs */
object = handle->object;
hwAttrs = handle->hwAttrs;

/* Disable preemption while checking if the SPI is open. */
key = Hwi_disable();

/* Check if the SPI is open already with the base addr. */
if (object->isOpen == true) {
Hwi_restore(key);

Log_warning1("SPI:(%p) already in use.", hwAttrs->baseAddr);

return (NULL);
}

/* Mark the handle as being used */
object->isOpen = true;
Hwi_restore(key);

Assert_isTrue((params->dataSize >= 4) &&
(params->dataSize <= 16), NULL);

/* Initialize the SPI object */
object->currentTransaction = NULL;
object->bitRate = params->bitRate;
object->dataSize = params->dataSize;
object->frameFormat = params->frameFormat;
object->mode = params->mode;
object->transferMode = params->transferMode;
object->transferTimeout = params->transferTimeout;
object->returnPartial = false;
#ifdef ***
object->wakeupCallbackFxn = NULL;
#endif

/* Determine if we need to use an 8-bit or 16-bit framesize for the DMA */
object->frameSize = (params->dataSize < 9) ? *** : ***;

Log_print2(Diags_USER2,"SPI:(%p) DMA buffer incrementation size: %s",
hwAttrs->baseAddr,
(object->frameSize) ? (UArg)"16-bit" : (UArg)"8-bit");

/* Register power dependency - i.e. power up and enable clock for SPI. */
Power_setDependency(hwAttrs->powerMngrId);

/* Configure the hardware module */
***(handle);

/* CSN is initialized using hwAttrs initially, but can be re-configured later */
object->csnPin = hwAttrs->csnPin;

/* Configure IOs after hardware has been initialized so that IOs aren't */
/* toggled unnecessary and make sure it was successful */
if (!***(handle)) {
/* Trying to use SPI driver when some other driver or application
* has already allocated these pins, error! */
Log_warning0("Could not allocate SPI pins, already in use.");

/* Release power dependency - i.e. potentially power down serial domain. */
Power_releaseDependency(hwAttrs->powerMngrId);

/* Mark the module as available */
key = Hwi_disable();
object->isOpen = false;
Hwi_restore(key);

/* Signal back to application that SPI driver was not succesfully opened */
return (NULL);
}

红色判断不通过, 返回NULL  不明白什么鬼 

用到了两个SPI接口

  • static bool ***(SPI_Handle handle) {
    *** *object;
    *** const *hwAttrs;
    PIN_Config spiPinTable[5];
    uint32_t i = 0;

    /* Get the pointer to the object and hwAttrs */
    object = handle->object;
    hwAttrs = handle->hwAttrs;

    /* Configure IOs */
    /* Build local list of pins, allocate through PIN driver and map HW ports */
    if (object->mode == SPI_SLAVE) {
    /* Configure IOs for slave mode */
    spiPinTable[i++] = hwAttrs->mosiPin | PIN_INPUT_EN;
    spiPinTable[i++] = hwAttrs->misoPin | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_INPUT_DIS | PIN_DRVSTR_MED;
    spiPinTable[i++] = hwAttrs->clkPin | PIN_INPUT_EN;
    spiPinTable[i++] = object->csnPin | PIN_INPUT_EN | PIN_PULLUP;
    }
    else {
    /* Configure IOs for master mode */
    spiPinTable[i++] = hwAttrs->mosiPin | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_INPUT_DIS | PIN_DRVSTR_MED;
    spiPinTable[i++] = hwAttrs->misoPin | PIN_INPUT_EN | PIN_PULLDOWN;

    /* Output low signal on SCLK until SPI module drives signal if clock polarity is configured to '0' */
    /* Output high signal on SCLK until SPI module drives signal if clock polarity is configured to '1' */
    if (object->frameFormat == SPI_POL0_PHA0 || object->frameFormat == SPI_POL0_PHA1) {
    spiPinTable[i++] = hwAttrs->clkPin | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_INPUT_DIS | PIN_DRVSTR_MED;
    }
    else {
    spiPinTable[i++] = hwAttrs->clkPin | PIN_GPIO_OUTPUT_EN | PIN_GPIO_HIGH | PIN_PUSHPULL | PIN_INPUT_DIS | PIN_DRVSTR_MED;
    }

    /* If CSN isn't SW controlled, drive it high until SPI module drives signal to avoid glitches */
    if(object->csnPin != PIN_UNASSIGNED) {
    spiPinTable[i++] = object->csnPin | PIN_GPIO_OUTPUT_EN | PIN_GPIO_HIGH | PIN_PUSHPULL | PIN_INPUT_DIS | PIN_DRVSTR_MED;
    }
    }
    spiPinTable[i++] = PIN_TERMINATE;

    /* Open and assign pins through pin driver */
    if (!(object->pinHandle = PIN_open(&(object->pinState), spiPinTable))) {
    return false;
    }

    /* Set IO muxing for the SPI pins */
    if (mode[object->mode] == SSI_MODE_SLAVE) {
    /* Configure IOs for slave mode */
    PINCC26XX_setMux(object->pinHandle, hwAttrs->mosiPin, (hwAttrs->baseAddr == SSI0_BASE ? IOC_PORT_MCU_SSI0_RX : IOC_PORT_MCU_SSI1_RX));
    PINCC26XX_setMux(object->pinHandle, hwAttrs->misoPin, (hwAttrs->baseAddr == SSI0_BASE ? IOC_PORT_MCU_SSI0_TX : IOC_PORT_MCU_SSI1_TX));
    PINCC26XX_setMux(object->pinHandle, hwAttrs->clkPin, (hwAttrs->baseAddr == SSI0_BASE ? IOC_PORT_MCU_SSI0_CLK : IOC_PORT_MCU_SSI1_CLK));
    PINCC26XX_setMux(object->pinHandle, object->csnPin, (hwAttrs->baseAddr == SSI0_BASE ? IOC_PORT_MCU_SSI0_FSS : IOC_PORT_MCU_SSI1_FSS));
    }
    else {
    /* Configure IOs for master mode */
    PINCC26XX_setMux(object->pinHandle, hwAttrs->mosiPin, (hwAttrs->baseAddr == SSI0_BASE ? IOC_PORT_MCU_SSI0_TX : IOC_PORT_MCU_SSI1_TX));
    PINCC26XX_setMux(object->pinHandle, hwAttrs->misoPin, (hwAttrs->baseAddr == SSI0_BASE ? IOC_PORT_MCU_SSI0_RX : IOC_PORT_MCU_SSI1_RX));
    PINCC26XX_setMux(object->pinHandle, hwAttrs->clkPin, (hwAttrs->baseAddr == SSI0_BASE ? IOC_PORT_MCU_SSI0_CLK : IOC_PORT_MCU_SSI1_CLK));
    if(object->csnPin != PIN_UNASSIGNED) {
    PINCC26XX_setMux(object->pinHandle, object->csnPin, (hwAttrs->baseAddr == SSI0_BASE ? IOC_PORT_MCU_SSI0_FSS : IOC_PORT_MCU_SSI1_FSS));
    }
    }

    return true;
    }

    红色执行错误,返回false

  • CC26X0的SPI操作,可以参考一下网友分享的代码:
    e2echina.ti.com/.../152483