我使用了CC2640R2F的硬件SPI对 9PIN的 OLED进行通信,这款OLED内含了GT20L16S1Y字库芯片和SSD1309。在发送数据给SSD1309能正常的显示BMP图片,
但是在显示中文的时候RX一直没有数据,在逻辑分析仪上已经显示成功切换片选切发送了数据,但是就是没有数据的返回。已知字库芯片上的最高支持的时钟频率为30MHZ,主机设置的params.bitRate = 300000。能分析分析到底是哪里出现问题了吗?
void OLED_WR_Byte(u8 dat,u8 cmd)
{
bool data_status = false;
if(CSNpin != OLED_CSN_STATUS)
{
//更换片选
SPI_control(handle, ***, &csnPin0);
CSNpin = OLED_CSN_STATUS;
}
transmitBuffer[0] = dat;
transaction.count = 1;
transaction.txBuf = transmitBuffer;
transaction.rxBuf = NULL;
transaction.arg = NULL;
if(cmd)
OLED_DC_Set();
else
{
OLED_DC_Clr();
}
// Open the SPI and perform the transfer
// handle = SPI_open(Board_SPI, ¶ms);
data_status = SPI_transfer(handle, &transaction);
if(data_status == false)
{
Log_error0("Error SPI_send!");
}
/* if(data_status == true && cmd == OLED_DATA)
{
// Log_info1("oled send msg: %u ",transmitBuffer[0]);
}*/
//拉高DC
OLED_DC_Set();
}
//发送一个字节到GT20L16S1Y
void Send_Command_to_ROM(u8 dat)
{
int ret;
if(CSNpin != ROM_CSN_STATUS)
{
//更换片选
ret = SPI_control(handle, ***, &csnPin1);
CSNpin = ROM_CSN_STATUS;
}
transmitBuffer[0] = dat;
transaction.count = 1;
transaction.txBuf = transmitBuffer;
transaction.rxBuf = NULL;
transaction.arg = NULL;
// Open the SPI and perform the transfer
// handle = SPI_open(Board_SPI, ¶ms);
SPI_transfer(handle, &transaction);
if(CSNpin == ROM_CSN_STATUS)
{
Log_info1("rom send msg: %u ",transmitBuffer[0]);
}
}
//从GT20L16S1Y获得一个字节
u8 Get_data_from_ROM(void)
{
int ret=0;
bool data_status = false;
u8 read=0;
if(CSNpin != ROM_CSN_STATUS)
{
ret = SPI_control(handle, ***, &csnPin1);
if(ret != SPI_STATUS_SUCCESS)
{
Log_error0("Error Get_data_from_ROM");
}
CSNpin = ROM_CSN_STATUS;
}
transaction.count = 1;
transaction.txBuf = NULL;
transaction.rxBuf = receiveBuffer;
data_status = SPI_transfer(handle, &transaction);
if(data_status == false)
{
Log_error0("Error SPI_send!");
}else
Log_info1("ROM_read_data %U",receiveBuffer[0]);
read = receiveBuffer[0];
return read;
}
最后是SPI的初始化:
SPI_init();
SPI_Params_init(¶ms);
params.bitRate = 300000;
params.frameFormat = SPI_POL0_PHA0;
params.mode = SPI_MASTER;
params.dataSize = 8;
handle = SPI_open(Board_SPI0, ¶ms);
if(handle == NULL)
{
Log_error0("Error SPI_open!");
}