This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CC1310的AES CBC加密密钥长度

Other Parts Discussed in Thread: CC1310

工程师您好,

我使用的文件为SDK中提供的CryptoCC26xx.h以及CryptoCC26xx.c,加密方式为AES-CBC,经过测试,密钥长度不能大于16字节,若大于16字节,也只会取前16字节作为密钥,请问CC1310的AES CBC加密密钥长度最多只能为16字节吗?能否修改为32字节吗?

  • The AES key is a shared secret between the two parties and has a length between 128, 192, or 256 bits

  • 我使用的文件为CryptoCC26XX.h / CryptoCC26xx.c,这个函数并不在这两个文件中,且我使用的工程是基于tirtos_cc13xx_cc26xx_2_21_00_06而非SDK,请问:
    1. 上述的密钥设置函数在哪个文件中?
    2. 能否直接使用CryptoCC26XX.h / CryptoCC26xx.c中的接口来设置密钥长度?若不能,请问以我目前的情况如何来修改密钥长度设置呢?
    感谢回答!
  • 以上来自CC1310 SDK的CC13XX driver library。正如之前回复的,请使用CC1310 sdk来实现相关功能
  • 由于时间原因,我们没有时间将目前的代码移植到SDK提供的工程中,且此前的产品是基于tirtos_cc13xx_cc26xx_2_21_00_06的(已有大量客户下单使用),所以想知道,根据目前的情况(使用tirtos_cc13xx_cc26xx_2_21_00_06,AES加密使用的CryptoCC26xx文件),如何修改密钥长度呢?
    感谢回答!