项目信息:
CCS910
SDK: simplelink_cc2640r2_sdk_3_40_00_10
从机运行的fimware:ble5_simple_peripheral
硬件板子: TI LaunchPad, 芯片是CC2640R2F
现象描述1:
四块开发板同时运行ble_5simple_perpheral程序,运行一段时间后从机无广播,并且主机scan不到从机。从设备供电电源连上示波器观察,没有正常的脉冲信号产生(正常广播会以一定的频率产生脉冲信号)。
目前在TI提供的ble_5simple_perpheral 只做了以下修改并且关闭了POWER_SAVE。
const PIN_Config BoardGpioInitTable[] = {
// CC2640R2_LAUNCHXL_PIN_RLED | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX, /* LED initially off */
// CC2640R2_LAUNCHXL_PIN_GLED | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX, /* LED initially off */
// CC2640R2_LAUNCHXL_PIN_BTN1 | PIN_INPUT_EN | PIN_PULLUP | PIN_IRQ_BOTHEDGES | PIN_HYSTERESIS, /* Button is active low */
// CC2640R2_LAUNCHXL_PIN_BTN2 | PIN_INPUT_EN | PIN_PULLUP | PIN_IRQ_BOTHEDGES | PIN_HYSTERESIS, /* Button is active low */
// CC2640R2_LAUNCHXL_SPI_FLASH_CS | PIN_GPIO_OUTPUT_EN | PIN_GPIO_HIGH | PIN_PUSHPULL | PIN_DRVSTR_MIN, /* External flash chip select */
CC2640R2_LAUNCHXL_UART_RX | PIN_INPUT_EN | PIN_PULLDOWN, /* UART RX via debugger back channel */
CC2640R2_LAUNCHXL_UART_TX | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL, /* UART TX via debugger back channel */
// CC2640R2_LAUNCHXL_SPI0_MOSI | PIN_INPUT_EN | PIN_PULLDOWN, /* SPI master out - slave in */
// CC2640R2_LAUNCHXL_SPI0_MISO | PIN_INPUT_EN | PIN_PULLDOWN, /* SPI master in - slave out */
// CC2640R2_LAUNCHXL_SPI0_CLK | PIN_INPUT_EN | PIN_PULLDOWN, /* SPI clock */
PIN_TERMINATE
};
现象描述2:
在TI提供的example (ble_5simple_perpheral)添加了一个周期时钟,每隔100毫秒去检测一次状态。
当从机运行一段时间后停止了广播,并且在周期时钟里面调用函数 uint8_t numActive = linkDB_NumActive(); 返回值是1.
uint8_t test_flag = 0;
static void SimplePeripheral_performMonitorTask(void)
{
uint8_t numActive = linkDB_NumActive();
if(numActive == 1)
{
ZHOU_SetIOValue(USER_OUTPUT_10,1);
}
else
{
ZHOU_SetIOValue(USER_OUTPUT_10,0);
}
if(test_flag == 0)
{
ZHOU_SetIOValue(USER_OUTPUT_9,1);
test_flag = 1;
}
else
{
ZHOU_SetIOValue(USER_OUTPUT_9,0);
test_flag = 0;
}
}