Hi 大神们,请教个问题。
MCU 是 CC2640R2F;
SDK 包是 simplelink_cc2640r2_sdk_4_20_00_04;
对于 simple_peripheral 和 simple_broadcaster 这两个,他们的 advertData[] 这个数组成员不一样,请问为什么成员会不一样?
如果我想把 simple_peripheral 的也改成 simple_broadcaster ,该怎样修改。
simple_peripheral 的 advertData[]
// Advertisement data (max size = 31 bytes, though this is
// best kept short to conserve power while advertising)
static uint8_t advertData[] =
{
// Flags: this field sets the device to use general discoverable
// mode (advertises indefinitely) instead of general
// discoverable mode (advertise for 30 seconds at a time)
0x02, // length of this data
GAP_ADTYPE_FLAGS,
DEFAULT_DISCOVERABLE_MODE | GAP_ADTYPE_FLAGS_BREDR_NOT_SUPPORTED,
// service UUID, to notify central devices what services are included
// in this peripheral
0x03, // length of this data
GAP_ADTYPE_16BIT_MORE, // some of the UUID's, but not all
LO_UINT16(SIMPLEPROFILE_SERV_UUID),
HI_UINT16(SIMPLEPROFILE_SERV_UUID)
};
simple_broadcaster 的 advertData[]
// GAP - Advertisement data (max size = 31 bytes, though this is
// best kept short to conserve power while advertisting)
static uint8 advertData[] =
{
// Flags; this sets the device to use limited discoverable
// mode (advertises for 30 seconds at a time) instead of general
// discoverable mode (advertises indefinitely)
0x02, // length of this data
GAP_ADTYPE_FLAGS,
GAP_ADTYPE_FLAGS_BREDR_NOT_SUPPORTED,
#ifndef BEACON_FEATURE
// three-byte broadcast of the data "1 2 3"
0x04, // length of this data including the data type byte
GAP_ADTYPE_MANUFACTURER_SPECIFIC, // manufacturer specific adv data type
1,
2,
3
#else
// 25 byte beacon advertisement data
// Preamble: Company ID - 0x000D for TI, refer to www.bluetooth.org/.../company-identifiers
// Data type: Beacon (0x02)
// Data length: 0x15
// UUID: 00000000-0000-0000-0000-000000000000 (null beacon)
// Major: 1 (0x0001)
// Minor: 1 (0x0001)
// Measured Power: -59 (0xc5)
0x1A, // length of this data including the data type byte
GAP_ADTYPE_MANUFACTURER_SPECIFIC, // manufacturer specific adv data type
0x0D, // Company ID - Fixed
0x00, // Company ID - Fixed
0x02, // Data Type - Fixed
0x15, // Data Length - Fixed
0x00, // UUID - Variable based on different use cases/applications
0x00, // UUID
0x00, // UUID
0x00, // UUID
0x00, // UUID
0x00, // UUID
0x00, // UUID
0x00, // UUID
0x00, // UUID
0x00, // UUID
0x00, // UUID
0x00, // UUID
0x00, // UUID
0x00, // UUID
0x00, // UUID
0x00, // UUID
0x00, // Major
0x01, // Major
0x00, // Minor
0x01, // Minor
0xc5 // Power - The 2's complement of the calibrated Tx Power
#endif // !BEACON_FEATURE
};