Other Parts Discussed in Thread: CC2640R2F, CC2640
Hi JRs:
请教下,CC2640R2F 通过什么工具可以写 UUID,有 SOP 吗?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kevin:
需要先给其中一块烧录host_test.hex文件充当central设备 =====》 这个有操作手册吗?
file:///C:/ti/peripheral_broadcast_sdk/docs/blestack/btool_user_guide/BTool_Users_Guide/index.html 没讲到,只是提到 More information on running this project can be found in the Bluetooth low energy Software Developer’s Guide and the Simple Peripheral sample application page.
请问是在 Bluetooth low energy Software Developer’s Guide 文档的哪一页?
谢谢
你可以參考一下
一開頭就寫到 "BTool is a PC Application that allows a user to form a connection between two BLE devices. BTool works by communicating with the CC2640R2F LaunchPad, acting as a network processor, by means of HCI vendor specific commands. This requires the CC2640R2F to be running the Host Test sample application."
Hi YiKai:
非常感謝您的解釋,我還想繼續請教下:
1. 您說的 LaunchPad 是 XDS110 嗎?
2. 我用的不是 XDS110 ,而是 XDS100 ,那 XDS100 可以替代 XDS110 嗎?
3. 如下圖左邊、中間 部分,是我們 Beacon 板子上 漏出來的幾個測點;
4. 我的 XDS100 和 Beacon 板子是通過 JTAG 的 TMS、TDO、TDI、TCK 連接的,XDS100 並沒有連 Beacon 板子的 UART RX、TX,請問這樣連接是正確的嗎?
5. serial-to-USB convertor 我用的是 FT232,是不是還要把 Beacon 板子的 UART RX、TX 連到 FT232 的 RX、TX 上?
6. 下圖右側,在裝置管理員里,XDS100 長出來的是 COM49,Serial-to-USB 長出來的是 COM50,我看文檔介紹,BTool 連的是 COM49,沒有連 COM50 ,那這個 COM50 是什麼時候用的?